5G NR
This topic describes the following RIM-RS properties, based on 3GPP 38.211 V17.2.0:
n_T_RIM Number of RIM-RS Transmission
Many of the channel types described in this topic provide a convenient channel editor, in table format, for convenient viewing and configuring of multiple channels. The editing functions for adding, removing, and copying rows appear directly above the editor. As you make edits, the Channel Allocation graph updates and, if a channel conflict occurs, an error message appears, describing the conflict.
Adds a new RIM-RS to the setup table. Supports up to 32 channels.
See also, Adding, Copying, and Deleting BWP or Channels.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS > + sign to Add |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs:ADD |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:ADD |
Deletes the currently selected RIM-RS from the setup table.
See also, Adding, Copying, and Deleting BWP or Channels.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS > + Elippsis icon > Delete |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs:DELete <integer> |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:DEL 1 |
Copies the currently selected RIM-RS to the last column of the setup table. Supports up to 32 channels.
See also, Adding, Copying, and Deleting BWP or Channels.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS > Elippsis icon > Copy |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs:COPY <integer> |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:COPY 1 |
Displays the existing PRS channels.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs:COUNt? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:COUN? |
Preset |
1 |
State Saved |
No |
Sets the name of the RIM-RS channel.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> General Settings > Name |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:NAME? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:NAME? |
Preset |
“RIM-RS0” |
State Saved |
Yes |
Enables or disables the channel or signal in a radio frame.
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> General Settings > Enabled |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>[:STATe] ON|OFF|1|0 [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>[:STATe]? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR? |
Preset |
0 |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> General Settings > Subcarrier Spacing |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SCSPacing SCS15K|SCS30K |
SCPI Example |
|
Preset |
“SCS30K” |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> General Settings > Power Boosting |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:POW <rel_ampl> |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:POW 2 |
Preset |
0 |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> General Settings > Cyclic Prefix |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:CPRefix NORMal|EXTended [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:CPRefix? |
SCPI Example |
|
Preset |
“NORM” |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Time-Frequency Resource Allocation > Allocated Slots |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SLOTs <string> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SLOTs? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:SLOT '0:2' |
Preset |
“0” |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Time-Frequency Resource Allocation > RB Number |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:RB:NUMBer <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:RB:NUMBer? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:RB:NUMB 48 |
Preset |
48 |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Time-Frequency Resource Allocation > Start PRB (RB Offset) |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:RB:OFFSet <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:RB:OFFSet? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:RB:OFFSet 10 |
Preset |
0 |
State Saved |
Yes |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Time-Frequency Resource Allocation > Start Symbol |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SYMBol:STARt <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SYMBol:STARt? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:SYMB:STAR 1 |
Preset |
0 |
State Saved |
Yes |
Min |
0 |
Max |
13 |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Sequence Generation > n_SCID |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SCIDn <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:SCIDn? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:SCID 3 |
Preset |
0 |
State Saved |
Yes |
Min |
0 |
Max |
1023 |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Sequence Generation > n_T_RIM Number of RIM-RS Transmission |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:NTRim <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:NTRim? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:NTR 3 |
Preset |
0 |
State Saved |
Yes |
Min |
0 |
Max |
2147483647 |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Sequence Generation > Multiplier Factor |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:MFACtor <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:MFACtor? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:MFAC 3 |
Preset |
1 |
State Saved |
Yes |
Min |
0 |
Max |
2147483647 |
GUI Location |
Apps > 5G NR > Carrier DL > Downlink > RIM-RS> Sequence Generation > Offset |
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:OFFSet <integer> [:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:RIMRs<channel>:OFFSet? |
SCPI Example |
RAD:NR5G:WAV:CCAR0:DLIN:RIMR:OFFS 3 |
Preset |
0 |
State Saved |
Yes |
Min |
0 |
Max |
2147483647 |